Custom Drive Scaling Attributes Dialog Box Overview (AXIS_SERVO_DRIVE)

Use this dialog box to monitor the position, velocity, acceleration, and torque scaling attributes or parameters for an axis of the type AXIS_SERVO_DRIVE.
When a parameter transitions to a read-only state, any pending changes to parameter values are lost, and the parameter reverts to the most recently saved parameter value.
When multiple workstations connect to the same controller using the Logix Designer application and invoke the Axis Wizard or Axis Properties dialog, the firmware allows only the first workstation to make any changes to axis attributes. The second workstation switches to a Read-Only mode, indicated in the title bar, so that you may view the changes from that workstation, but not edit them.
Parameters
Advanced Custom Scaling
Use this dialog box to display internal SERCOS position, velocity, acceleration and torque scaling attributes established by the ControlLogix system for an axis of the type AXIS_SERVO_DRIVE.
Attribute/Parameter
Description
PositionDataScaling
This 16-bit attribute displays the scaling method used on position values, e.g., Position Command Value, Position Feedback Value 1 (Motor Feedback), and Position Feedback Value 2 (Auxiliary Feedback). Because only the first 8 bits (0 - 7) of this attribute are used (8 - 15 are reserved), decimal values of this attribute range from 0 to 255.
Bit values are:
Bits 2-0: Scaling method
000 - no scaling
001 - linear scaling
010 - rotational scaling
Bit 3:
0 - preferred scaling
1 - parameter scaling
Bit 4: Linear Units
0 - meters
1 - inches
Bit 4: Units (must be 0)
0 - degrees
1 - (reserved)
Bit 5: (reserved)
Bit 6: Data reference
0 - at the motor shaft
1 - at the load
Bit 7: Processing format
0 - absolute format
1 - modulo format
PositionDataScalingFactor
This 16 bit unsigned attribute displays the scaling factor for all position data in a drive, with decimal values ranging from 1 to 2^16-1.
PositionDataScalingExp
This 16 bit unsigned attribute displays the scaling exponent for all position data in a drive, with decimal values ranging from -2^15 to 2^15-1.
Bit values are:
Bit 14-0: Exponent value
Bit 15: Exponent sign:
0 - Positive
1 - Negative
VelocityDataScaling
This 16-bit attribute displays the scaling method to use on velocity values (e.g., Velocity command value, Velocity feedback value, and Homing Velocity), with decimal values ranging from 0 to 127.
Bit values are:
Bits 2-0: Scaling method
000 - no scaling
001 - linear scaling (not supported)
010 - rotational scaling
Bit 3:
0 - preferred scaling
1 - parameter scaling
Bit 4: Units for rotary
0 - revolutions
1 - (reserved)
Bit 4: Units linear
0 - meters
1 - inches
Bit 5: Time
0 - minutes
1 - seconds
Bit 6: Data reference (must be 0)
0 - at the motor shaft
1 - at the load (not implemented)
All other bits are reserved.
VelocityDataScalingFactor
This 16-bit attribute displays the scaling factor for all velocity data. Decimal values for this attribute range from 1 to (2^16)-1.
VelocityDataScalingExp
This 16-bit attribute displays the scaling exponent for all velocity data. Decimal values for this attribute range from -2^15 to (2^15)-1.
AccelerationDataScaling
This 16-bit attribute displays the scaling method to use on acceleration values, with decimal values ranging from 0 to 127.
Bit values are:
Bits 2-0: Scaling method
000 - no scaling
001 - linear scaling
010 - rotational scaling
Bit 3:
0 - preferred scaling
1 - parameter scaling
Bit 4: Units
0 - radians
1 - (reserved)
Bit 5: Time
0 - seconds
1 - (reserved)
Bit 6: Data reference
0 - at the motor shaft
1 - at the load (not implemented)
All other bits are reserved.
AccelerationDataScalingFactor
This 16 bit unsigned attribute displays the scaling factor for all acceleration data in a drive, with decimal values ranging from 1 to (2^16)-1.
AccelerationDataScalingExp
This 16 bit unsigned attribute displays the scaling exponent for all acceleration data in a drive, with decimal values ranging from -2^15 to (2^15)-1.
Bit values are:
Bit 14-0: Exponent value
Bit 15: Exponent sign:
0 - Positive
1 - Negative
TorqueDataScaling
This 16-bit attribute displays the scaling method to use on torque values (e.g. , Torque Command Value, and Bipolar torque limit value) with decimal values ranging from 0 to 127.
Bit values are:
Bits 2-0: Scaling method
000 - percentage scaling
001 - linear scaling (force)
010 - rotational scaling (torque)
Bit 3:
0 - preferred scaling
1 - parameter scaling
Bit 4: Units
0 - Newton meter (Nm)
1 - inch pound force (lbf)
Bit 5: (reserved)
Bit 6: Data reference
0 - at the motor shaft
1 - at the load
All other bits are reserved.
TorqueDataScalingFactor
This 16 bit unsigned attribute displays the scaling factor for all torque data in a drive, with decimal values ranging from 1 to (2^16)-1.
TorqueDataScalingExp
This 16 bit unsigned attribute displays the scaling exponent for all torque data in a drive, with decimal values ranging from -2^15 to (2^15)-1.
Bit values are:
Bit 14-0: Exponent value
Bit 15: Exponent sign:
0 - Positive
1 - Negative
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal