Coordinate System Properties - Offsets

Use the settings on the
Offsets
tab in the
Coordinate System Properties
dialog box to define the end effector and base offset values for the robotic arm.
The
Offset
tab shows the views of a typical robotic arm based on the configuration of the robot geometry type on the
General
tab. The type of offsets and the number of available offsets is determined by the coordinate system and the number of axes associated with the coordinate system.
When specifying the end effector and base offset values, be sure that the values are calculated using the same measurement units as the linked Cartesian coordinate system. For example, if the manufacturer specifies the robot offset using millimeter units and you want to configure the robot using inches, then convert the millimeter link measurements to inches and enter the values in the appropriate offset fields.
TIP: To open the Offsets tab:
  1. In the
    Controller Organizer
    , expand the
    Motion Group
    folder, and double-click the coordinate system.
  2. On the
    Coordinate System Properties
    dialog box, select the
    Offsets
    tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal