Torque/Current Loop page
Use the settings on the
Torque/Current Loop
page in the Axis Properties dialog box to configure the torque and current loop of the axis.
TIP:
To open the Torque/Current Loop page:
- In theController Organizer, expand theMotion Groupsfolder, then right-click the axis and selectProperties.
- From theAxis Propertiesdialog box, inCategories, selectTorque/Current Loop.
Parameter | Description |
|---|---|
Gains Bandwidth | Enter a value for the bandwidth in Hertz. |
Integral Time Constant | Enter a value for the integral time constant in seconds. |
Peak Torque Limit Positive | Enter a value for the positive peak current limit as a percent rated of the motor. |
Peak Torque Limit Negative | Enter a value for the negative peak current limit as a percent rated of the motor. |
Motor Overload Limit | Enter a value for the motor overload limit as a percent rated of the motor. |
Parameters | Opens the Motion Axis Parameters page to modify existing or additional parameters.
TIP:
The
Parameter List page may contain more
attributes than the associated page. In some cases, attributes that display on the
Parameter List page do not display on the associated page. |
Provide Feedback