Select the Catalog Number as the data source
Using the
Motor
tab, specify where the motor configuration values are originating by selecting a motor by catalog number from the Motion Database.To select the Catalog Number as the data source:
- In theAxis Propertiesdialog box, in theCategoriespane,clickMotor.
- In theMotor Device Specificationarea, from theData Sourcelist, clickCatalog Number.
- ClickChange Catalog.
- In theChange Catalog Numberdialog box, select a motor and clickOK. TheNameplate/Datasheet - Phase to Phaseparameters are populated with the parameter information for the selected motor.
- ClickApplyto apply the changes.
TIP:
When using a motor catalog number as the data source,
default values, for example, gains and dynamics, are automatically set based on the
Application Type and Loop Response
settings from the General
tab. Using
default values minimizes the need for adjusting these parameters using autotune, manual
tune, and the manual setting of these parameters.Provide Feedback