Motor page
Use the
Motor
page to select the data source to enter information about the motor or drive.
NOTE:
The parameters available on the
Motor
page depend on the Data Source
and Motor Type
.
TIP:
To open the Motor page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickMotor.
Parameter | Description |
Data Source | Specifies the data source where the motor configuration values originate. The available data sources are:
Select Nameplate Datasheet to enable the Nameplate/Datasheet parameter section and configure motor options.
TIP:
The
Nameplate / Datasheet - Phase to
Phase parameters changes based on the motor type selection. Similar entry
fields also map to different attributes.The Nameplate/Datasheet parameters are only available when selecting the Nameplate Datasheet data source.The options for Data Source vary by drive. The motor data resets to the default settings when changing the data source value. |
Catalog Number | Identifies the current motor catalog number. If Data Source is set to Catalog Number , this field is read only and displays the catalog number selected from the Change Catalog Number dialog box. If Data Source is set to a value other than Catalog Number , this control is set to <none> .The TrackMoverMotor or TrackSection Catalog Number:
All datasheet entry fields are read only. When Data Source is set to Motor NV , the applicable parameters display in the Nameplate/Datasheet - Phase to Phase parameters section.Select a catalog number that matches the motor associated with this axis. Select the Parameters button to view the Motion Axis Parameters associated with that catalog number in the motion database. |
Change Catalog | Opens the Change Catalog Number dialog box. Use the Change Catalog Number dialog box to select a different catalog number for the motor. The Change Catalog button appears dimmed if Data Source is set to a value other than Catalog Number . |
Motor Type | Select the type of motor that is associated with this axis. This parameter is enabled when Data Source is set to Nameplate Datasheet .If Data Source is set to Catalog Number , Motor Type appears dimmed and is read-only. The motor type associated with the catalog number is defined in the motion database. If Catalog Number is set to <none> , Motor Type is set to Not Specified .If Data Source is set to Drive NV or Motor NV , Motor Type is set to Not Specified .If Motor Type is enabled, the options are:
The options available for Motor Type may be limited based on the drive selected. |
Units | Displays the measurement units used for the selected motor type. Units is enabled when Data Source is set to Drive NV or Motor NV . When Data Source is set to Catalog Number , the units are set from the motor database.If Units is enabled, the options are:
|
Nameplate/Datasheet - Phase to Phase parameters | The Nameplate/Datasheet section of the page changes based on the Motor Type selection. Also, similar entry fields may be mapped to different attributes.
TIP:
These controls only display when a motor type
has been selected.
|
Rated Power | Specifies the nameplate rated power for the motor in kilowatt (Kw) units. |
Rated Voltage | Specifies the nameplate AC voltage rating of the motor in volts (RMS). |
Rated Speed | Specifies the nameplate rated speed of the motor. The units are reported in meters per second (m/s). |
Rated Current | Specifies the rated current of the motor in amps (RMS). |
Rated Force | Specifies the nameplate continuous force of a linear permanent magnet motor. The units are reported in newtons (N). |
Rated Torque | For the Rotary Permanent Magnet motor type, specifies the rated torque in N-m units. |
Pole Count | For Rotary Permanent Magnet and Rotary Induction motor types, specifies the pole count of the motor. |
Pole Pitch | Specifies the pole pitch of a linear motor. The units are reported in millimeters (mm). |
Track Mover Length | The physical length in meters (m) of a mover. Use the physical length measurement for programming multiple movers on the track. |
Rated Frequency | Specifies the nameplate frequency rating of an induction motor in Hertz (Hz). |
Max Speed | Specifies the maximum safe speed of the motor in RPMs. The units are reported in meters per seconds (m/s). |
Peak Current | Specifies the peak or intermittent current rating of the motor in amps (RMS). |
Motor Overload Limit | Specifies the maximum thermal overload limit for the motor. The value, which is typically 100%, corresponds to the power dissipated when operating at the continuous rating of the motor. |
Extended Speed Permissive | Determines whether the Bus Overvoltage Speed Limit is applied to the velocity limiter. Select the check box to remove the velocity limit protection against Bus Overvoltage conditions associated with permanent magnetic motors. Clear the check box to enable the velocity limit protection. |
Bus Overvoltage Speed | Limits the magnitude of the velocity reference value allowed into the velocity summing junction to protect drive from damage from bus overvoltage conditions that can occur when disabling a moving permanent magnetic motor. If the signal entering the velocity limiter exceeds the velocity limit value, and the Extended Speed Permissive check box is cleared, the velocity limiter clamps the velocity reference to this value and sets the Velocity Limit status bit. If the Extended Speed Permissive check box is selected, or the value of this attribute is 0, this limit is not applied. The units are reported in meters per seconds (m/s).This parameter is read-only. |
Max Extended Speed | Establishes a limit on the magnitude of the velocity reference value allowed into the velocity summing junction to protect the motor from damage due to an over-speed condition. The units are reported in meters/second (m/s). |
Parameters | Opens the Motion Axis Parameters page to modify existing or additional parameters.
TIP:
The
Parameter List page may contain more
attributes than the associated page. In some cases, attributes that display on the
Parameter List page do not display on the associated page. |
Provide Feedback