Unschedule a program/phase
Unschedule a program or phase so it does not run in any task.
To move a program/phase from one task to another, unschedule the program or phase from the first task, and then schedule it in the other.
To unschedule a program/phase:
- From theController Organizerright-click the task to unschedule the program/phase, and chooseProperties.TheTask Propertiesdialog appears.
- Select theProgram/Phase Scheduletab.TIP:Only Safety programs are scheduled in the Safety task, and standard programs in standard tasks. Because of this, when you select a Safety task, only Safety programs appear in this dialog. If you choose any other type of task, only standard programs appear.
- Select the program/phase to unschedule from theScheduledlist.
- SelectRemove.The program/phase moves to theUnscheduledlist.
- SelectApplyto unschedule the program/phase.The program/phase displays under theUnscheduled Programsfolder in theController Organizer.
Provide Feedback