Delete a tag
Use these steps to delete a tag.
IMPORTANT:
Undo
is not available after you delete a tag.To delete a tag
- Double click theController TagsorProgram Tagsfolder, under the specified program, to open the tag collection.
- Select theEdit Tagstab.
- Set the filter toShow All.
- If you wish to delete all tags, from theEditmenu, chooseSelect All.If you wish to delete only one tag or several contiguous tags, select your left mouse button in the selection column, and drag it over the tags you wish to delete to select them.
- From theEditmenu, chooseDelete.
Provide Feedback