Expand and collapse code segments in the Structured Text editor
Automatic outlining organizes a Structured Text routine into collapsible segments. Use
Expand All Outlining
and Collapse All Outlining
to quickly expand or collapse all the segments in a routine.To expand and collapse code segments:
- On the main menu, select selectEdit > Outlining > Expand All Outliningto expand all segments in the routine. SelectEdit > Outlining > Collapse All Outliningto collapse all segments.
- To toggle a segment from expanded to collapsed, selectEdit > Outlining > Toggle Current Outlining.
Provide Feedback