Sequence Summary Control table columns
These columns are displayed in the
Equipment Sequence
list in the table area of the Sequence Summary Control. The list can be sorted in alphabetical order for any column to group Equipment Sequence
s based on status.Status column | Description |
Sequence Name | The Equipment Sequence name. |
ID | The identifier assigned to the Equipment Sequence before it runs. This field is editable when the sequence is inactive, or in the IDLE state. When the sequence is active, the ID field is locked. |
State | The current execution state of the Equipment Sequence . Possible states include NOT CONNECTED, IDLE, RESTARTING, RUNNING, RESETTING, HOLDING, STOPPING, ABORTING, HELD, STOPPED, ABORTED, and COMPLETE. |
Mode | The operational mode for the Equipment Sequence , either Automatic , in which sequence steps advance automatically, or Manual , in which the operator advances sequence steps manually. |
Phase Failure | Indicates a failure in an Equipment Phase associated with the sequence. |
Sequence Failure | Indicates a failure in the Equipment Sequence . |
Owners | The current owner of the Equipment Sequence . |
Unit ID | A numerical representation of the piece of equipment that the Equipment Sequence is controlling. |
Provide Feedback