Configure the Sequence Parameters Control
To configure the
Sequence Parameters Control,
you need to customize several settings in the Property Panel
for the control.You can configure the
Sequence Parameters Control
to communicate with a controller, to use VBA scripting, or (to) change display options.Prerequisites
- Open theFactoryTalk ViewSite Edition (SE) application.
- Open a display that contains theSequence Parameters Control.
Provide Feedback