Configure the Sequence Parameters Control display options
To configure the Sequence Parameters Control display options
- Right-click theSequence Parameters Controlin the display window.
- SelectProperty Panel.
- Select optional display options as needed:
- (optional) In theColumn1Contentproperty text box, select a content option for the column.
- (optional) In theColumn2Contentproperty text box, select a content option for the column.
- (optional) In theColumn3Contentproperty text box, select a content option for the column.
- (optional) In theColumn4Contentproperty text box, select a content option for the column.
- (optional) In theColumn5Contentproperty text box, select a content option for the column.
- (optional) In theColumn6Contentproperty text box, select a content option for the column.
- (optional) In theColumn7Contentproperty text box, select a content option for the column.
- (optional) In theColumn8Contentproperty text box, select a content option for the column.
- (optional) In theCurrentFilterproperty text box, select an option to filter the display to Sequence Parameters, step tags, selected steps, active steps, or all.
- (optional) In theShowFilterproperty text box, selectTrueto display the filter control.
- (optional) In theShowSequenceHeaderproperty text box, selectTrueto display the sequence header.
- (optional) In theShowStatusBarproperty text box, selectTrueto display the status bar.
- (optional) In theSortFieldproperty text box, select an option to sort by that field.
- (optional) In theSortOrderproperty text box, select an option to sort ascending or descending.
- (optional) In theTouchPointerSizeproperty text box, select an option to auto-size, decrease, or increase the size of buttons.
- Close theProperty Panelwindow.
- SelectSave.
Provide Feedback