Configure the Min and Max values

To configure the Minimum and Maximum va
l
ues for a Sequence tag input/output Parameters in
Studio 5000
.
  1. Using
    Studio 5000
    , select the tag or parameter. Supported data types are INT, SINT, DINT, and REAL.
  2. Enable extended properties and select Minimum and Maximum.
  3. Assign values to Minimum and Maximum.
  4. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal