XYMinMaxOption constant
Use the constant to specify the option of the minimum and maximum y-axis scale.
MinMaxOptionAutomatic
(0) - The scale option is Automatic
.MinMaxOptionValue
(1) - The scale option is Minimum
and Maximum
values.MinMaxOptionTagProperties
(2) - The scale option is Use tag Min and Max properties
.Provide Feedback