WindowBackColor property (XY Plot object)
Returns or sets the background color of the runtime chart area. Read/write. OLE_COLOR.
OLE_COLOR is a type definition that resolves to a Long.
Syntax
XYPlot1
.WindowBackColor
[= value
]where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.value
- is an RGB color value that specifies the background color of the chart area.Example
Private Sub SetWindowBackColor() XYPlot1.WindowBackColor = RGB(0,0,0) End Sub
Provide Feedback