TrendStackAxesMode constant (XY Plot object)

Use the constant to specify the axes stake mode.
Stack_Both
(3) - Both x-axes and y-axes are stacked.
Stack_None
(0) - No axes are stacked.
Stack_X
(1) - The x-axes are stacked.
Stack_Y
(2) - The y-axes are stacked.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal