TransposeAxes method

Switches the x-axis with the y-axis.
Syntax
XYPlot1
.
TransposeAxes
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
Example
Private Sub btnTransposeAxes() XYPlot1.TransposeAxes End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal