RubberbandZoomEnable property (XY Plot object)

Returns or sets a value that indicates whether rubberband zoom is enabled. Read/write. Boolean.
Syntax
XYPlot1
.
RubberbandZoomEnable
[ = value]
where
XYPlot1 -
is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
value -
is a Boolean value that specifies whether RubberbandZoomEnable is True or False.
Example
Private Sub SetRubberbandZoomEnable() XYPlot1.RubberbandZoomEnable = True End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal