ResetZoom method (XY Plot object)

Resets the chart zoom.
Syntax
XYPlot1
.
ResetZoom
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
Example
Private Sub btnResetZoom() XYPlot1.ResetZoom End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal