CustomFileExplorer property (XY Plot object)
Returns or sets whether the custom file explorer or Windows file explorer opens when saving the trace data or captured image. Read/write. Boolean.
Syntax
XYPlot1
.CustomFileExplorer
[ = state
]where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.state
- is a parameter of the type Boolean that can be set to one of the following:- True: The custom file explorer opens.
- False: The Windows file explorer opens.
Example
Private Sub SetCustomFileExplorer() XYPlot1.CustomFileExplorer = True End Sub
Provide Feedback