CollapseNSExplorer property (XY Plot object)

Returns or sets whether to collapse the tag explorer. Read/write. Boolean.
Syntax
XYPlot1
.
CollapseNSExplorer
[=
state
]
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
state
- is a parameter of the type Boolean that can be set to one of the following:
  • True
    : Collapses the tag explorer and shows the title only.
  • False
    : Expands the tag explorer.
Example
Private Sub CollapseNSExplorer() 'Collapses the tag explorer. XYPlot1.CollapseNSExplorer = False End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal