ChartStyle property (XY Plot object)

Returns the type of the runtime chart. Currently the only style supported is "
XY Plot
". Read only. String.
Syntax
XYPlot1
.
ChartStyle
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
Example
Private Sub GetChartStyle() Dim str As String str = XYPlot1.ChartStyle End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal