ChartLiveMode property (XY Plot object)

Returns or sets whether the traces in the runtime chart will update automatically or will require manual updates. Read/write. Boolean.
Syntax
XYPlot1
.
ChartLiveMode
[ =
state
]
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
state
- is a parameter of the type Boolean that can be set to one of the following:
  • True
    . Traces in the chart will automatically update at the rate set in the XY Plot's properties.
  • False
    . Traces in the chart will not automatically update. Traces may be manually updated by using the
    Refresh
    button on the toolbar.
Example
Private Sub SetChartLiveMode() XYPlot1.ChartLiveMode = True End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal