ActiveYAxisScalingMode property (XY Plot object)

Returns or sets the y-axis scaling mode for the current tag in the runtime chart. Read/write. Single.
Syntax
XYPlot1
.
ActiveYAxisScalingMode
[ =
value
]
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
value
– is a parameter of the type Single that specifies the y-axis scaling mode:
  • Automatic
    = 0
  • Manual
    = 1
  • UseTagMinMax
    = 2
  • UseTagValue
    = 3
Example
Private Sub SetActiveYAxisScalingMode() XYPlot1.ActiveYAxisScalingMode = 1 End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal