ActiveYAxisMaxValue property (XY Plot object)

Returns or sets the maximum value of the y-axis for the current tag in the runtime chart. Read/write. Single.
TIP:
This property will be implemented in a future release.
Syntax
XYPlot1
.
ActiveYAxisMaxValue
[ =
value
]
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
value
- is a parameter of the type Single that specifies the y-axis maximum value.
Example
Private Sub SetActiveYAxisMaxValue() XYPlot1.ActiveYAxisMaxValue = 100 End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal