ActiveYAxisLineWidth property (XY Plot object)

Returns or sets the width of the y-axis line for the current tag in the runtime chart. Read/write. Long.
Syntax
XYPlot1
.
ActiveYAxisLineWidth
[=
value
]
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
value
- is a long value that specifies the width of the y-axis line. The minimum value is 1, and maximum value is 10.
Example
Private Sub SetActiveYAxisLineWidth() XYPlot1.ActiveYAxisLineWidth = 2 End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal