ActiveTraceLineWidth property (XY Plot object)

Returns or sets the width of the line for the selected trace in the runtime chart. Read/write. Long.
Syntax
XYPlot1
.
ActiveTraceLineWidth
[ =
value
]
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
value
- is a parameter of the type Long that specifies the width of the trace line. The minimum value is 1, and the maximum value is 10.
Example
Private Sub SetActiveTraceLineWidth() XYPlot1.ActiveTraceLineWidth = 2 End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal