ActiveTraceLineDashStyle property (XY Plot object)
Returns or sets the line dash style for the selected trace. Read/write. Long.
Syntax
XYPlot1
.ActiveTraceLineDashStyle
[ = value
]where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.value
- is a parameter of the type Long that specifies the line dash style. Valid values are:- Solid = 0
- Dash = 1
- Dot = 2
- Dashdot = 3
- DashDotDot = 4
Example
Private Sub SetActiveTraceLineDashStyle() XYPlot1.ActiveTraceLineDashStyle = 1 End Sub
Provide Feedback