TimePeriodStart property (TrendPro object)

Returns or sets the start date and time for the current time period. To set this property, the TimePeriodAbsoluteMode property must be set to
True
. Read/write. String.
Syntax
TrendPro1
.
TimePeriodStart
[ =
value
]
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
value -
is a parameter of the type String. This is a date/time string such as "2016/01/01 12:00 PM".
Example
Private Sub SetTimePeriodStart() TrendPro1.TimePeriodAbsoluteMode = True TrendPro1.TimePeriodStart = "2016/01/01 09:15 AM" End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal