StackAxesMode property (TrendPro object)

Returns or sets whether the axes are stacked on the plot surface.
Syntax
TrendPro1
.
StackAxesMode
(Long
stackType
)
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
stackType
- is a Long value that specifies how the axes are stacked. The valid values are:
  • 0
    : No axes are stacked.
  • 1
    : The x-axes are stacked.
  • 2
    : The y-axes are stacked.
  • 3
    : Both x-axes and y-axes are stacked.
Example
Private Sub StackAxesMode() TrendPro1.StackAxesMode = 2 End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal