SingleTraceMode property (TrendPro object)
Returns or sets whether the single trace mode is on. Read/write. Boolean.
Syntax
TrendPro1
.SingleTraceMode
[= state
]where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.state - is a parameter of the type Boolean that can be set to one of the following:
- True: Turns on the single trace mode at runtime.
- False: Turns off the single trace mode at runtime.
Example
Private Sub SingleTraceMode() TrendPro1.SingleTraceMode = True End Sub
Provide Feedback