ShowNSExplorer property (TrendPro object)
Returns or sets whether the tag explorer is displayed. Read/write. Boolean.
Syntax
TrendPro1
.ShowNSExplorer
[= state
]where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.state
- is a parameter of the type Boolean that can be set to one of the following:- True: Shows the tag explorer at runtime.
- False: Does not show the tag explorer at runtime.
Example
Private Sub ShowNSExplorer() TrendPro1.ShowNSExplorer = True End Sub
Provide Feedback