ShowAlarmCursor property

Returns or sets whether the alarm event time is displayed when you click the alarm event on the trace. Read/write. Boolean.
Syntax
TrendPro1
.
ShowAlarmCursor
[=
state
]
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
state
- is a parameter of the type Boolean that can be set to one of the following:
  • True
    : Shows the alarm event time.
  • False
    : Collapses and does not show the alarm event time.
Example
Private Sub btShowAlarmCursor_Click() TrendPro1.ShowAlarmCursor = False End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal