SetAlarmEventSort method
Sorts the alarm event list by a specified attribute.
Syntax
TrendPro1
.SetAlarmEventSort
(String attribute
, Long sortType
)where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.attribute
- is the name of a alarm event attribute. The value is not case-sensitive. It must be one of Priority
, EventTime
, AlarmName
, and AlarmState
.sortType
- is a Long value that specifies the sort order. The valid values are:- 0: not sorting
- 1: ascending
- 2: descending
Example
Private Sub btnSortByTime() TrendPro1.SetAlarmEventSort "EventTime", 1 End Sub
Provide Feedback