RubberbandZoomEnable property (TrendPro object)

Returns or sets a value that indicates whether rubberband zoom is enabled. Read/write. Boolean.
Syntax
TrendPro1
.
RubberbandZoomEnable
[ = value]
where
TrendPro1 -
is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
value -
is a Boolean value that specifies whether RubberbandZoomEnable is True or False.
Example
Private Sub SetRubberbandZoomEnable() TrendPro1.RubberbandZoomEnable = True End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal