MinMaxOption constant

Use the constant to specify the option of the minimum and maximum y-axis scale.
MinMaxOptionAutomatic
(0) - The scale option is
Automatic
.
MinMaxOptionValue
(1) - The scale option is
Minimum
and
Maximum
values.
MinMaxOptionTagProperties
(2) - The scale option is
Use tag Min and Max properties
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal