DeleteTemplate method (TrendPro object)
Deletes the specified template.
Syntax
TrendPro1
.DeleteTemplate
TemplateName
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.TemplateName
- is a parameter of the type String that specifies the name of the template.Example
Private Sub btnDeleteTemplate() TrendPro1.DeleteTemplate "MyTemplate" End Sub
Provide Feedback