CollapseNSExplorer property (TrendPro object)

Returns or sets whether to collapse the tag explorer. Read/write. Boolean.
Syntax
TrendPro1
.
CollapseTagExplorer
[=
state
]
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
state
- is a parameter of the type Boolean that can be set to one of the following:
  • True
    : Collapses the tag explorer and shows the title only.
  • False
    : Expands the tag explorer.
Example
Private Sub CollapseTrendProExplorer() 'Collapses the tag explorer. TrendPro1.CollapseTagExplorer = False End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal