ChartTitle property (TrendPro object)

Returns or sets a value for a title that is displayed on the chart. Read/write. String.
Syntax
TrendPro1
.
ChartTitle
[=
title
]
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
title - is a parameter of the type String that specifies the chart title.
Example
Private Sub ShowTitle() TrendPro1.ChartTitle = "My Chart Title" End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal