ButtonID constant
Use the constant to specify the buttons on the toolbar.
AlarmCursor
(33)ApplyTemplate
(37)AutoScale
(19)DeleteTemplate
(38)DeleteTrace
(17)HideTrace (22)
Highlight
(23)LiveMode
(9)NewButton
(1)NewTimePeriod
(25)NextTimePeriod
(26)NextTrace
(16)PreviousTrace
(15)PrintButton
(4)PrintPreview
(6)Refresh
(7)RubberBandZoom
(29)SaveTemplate
(36)SingleTrace
(21)StackEventY
(34)StackY
(20)Statistics
(13)XCursors
(11)YCursors
(12)Provide Feedback