AutoScale property (TrendPro object)

Returns or sets whether the runtime chart will auto scale the y-axis. Read/write. Boolean.
Syntax
TrendPro1
.
AutoScale
[ =
state
]
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
state
- is a parameter of the type Boolean that can be set to one of the following:
  • True
    . Chart will automatically scale the y-axis.
  • False
    . Chart will not automatically scale the y-axis.
Example
Private Sub SetAutoScale() TrendPro1.AutoScale = True End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal