AddTimePeriod method (TrendPro object)
Adds a new time period to the runtime chart. Time periods may be specified in one of two ways: as an absolute time period between two specified dates and times or as a specified number of seconds, minutes, or hours relative to the current time.
Syntax
TrendPro1
.AddTimePeriod
start
, end
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.start
– is a parameter of the type String. If an absolute time period is desired, then this will be a date/time string such as "2016/01/01 12:00 PM
". If a relative time period is desired then this string must be set to "REL
".end
– is a parameter of the type String. If an absolute time period is desired, then this will be a date/time string such as "2016/02/01 12:00 PM
". If a relative time period is desired then this string represents the relative amount of time from the current time.Relative times are specified in the format
sNu
()
where:- s- direction. Only "–" (minus sign) is supported.
- N -duration.
- u- duration units.smeans seconds,mmeans minutes, andhmeans hours.
Examples of relative times:
- -10m(): means last ten minutes
- -2h(): means last two hours
- -168h(): means last week
Example
Private Sub btnAddTimePeriod() Rem Add an absolute time period. TrendPro1.AddTimePeriod "2016/01/01 09:15 AM", "2016/02/01 10:00:05 PM" Rem Add a relative time period for the last ten minutes. TrendPro1.AddTimePeriod "REL", "-10m()" End Sub
Provide Feedback