ActiveYAxisMinValue property (TrendPro object)
Returns or sets the minimum value of the y-axis for the current tag in the runtime chart. Read/write. Single.
TIP:
This property will be implemented in a future release.
Syntax
TrendPro1
.ActiveYAxisMinValue
[ = value
]where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.value
– is a parameter of the type Single that specifies the y-axis minimum value.Example
Private Sub SetActiveYAxisMinValue() TrendPro1.ActiveYAxisMinValue = 100 End Sub
Provide Feedback