ActiveXAxisMajorTickScale property (TrendPro object)

Returns or sets the x-axis major tick scale in the runtime chart. Read/write. Single.
Syntax
TrendPro1
.
ActiveXAxisMajorTickScale
[=
value
]
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
value
- is a parameter of the type Single that specifies the x-axis major tick scale. The minimum value is 0, and the maximum value is the upper limit of a Single data type.
Example
Private Sub SetActiveXAxisMajorTickScale() TrendPro1.ActiveXAxisMajorTickScale = 2 End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal