ActiveTraceLineColor property (TrendPro object)

Returns or sets the color of the trace line for the selected trace. Read/write. OLE_COLOR.
OLE_COLOR is a type definition that resolves to a Long.
Syntax
TrendPro1
.
ActiveTraceLineColor
[ =
value
]
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
value
- is an RGB color value that specifies the color of the trace line.
Example
Private Sub SetActiveTraceLineColor() TrendPro1.ActiveTraceLineColor = RGB(0,0,0) End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal