ActiveTraceIndex property (TrendPro object)

Returns a value indicating which trace in the chart is active. Read-only. Long.
Syntax
TrendPro1
.
ActiveTraceIndex
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
value
- is a parameter of the type Long that returns the active index for the selected trace. The first active index has an index value of zero. If there is no active trace, a -1 is returned.
Example
Private Sub SetActiveTraceIndex() Dim index As Long index = TrendPro1.ActiveTraceIndex End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal