ActivePlottingAlgorithmLinear property (TrendPro object)

Returns or sets whether a linear plotting algorithm or a sample and hold plotting algorithm is used. Read/write. Boolean.
Syntax
TrendPro1
.
ActivePlottingAlgorithm
[ =
state
]
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
state -
is a parameter of the type Boolean that can be set to one of the following:
  • True
    : Applies a linear plotting algorithm, which connects data points in a progressive line.
  • False
    : Applies a sample and hold plotting algorithm, which draws flat lines between time periods and makes adjustments along the y-axis when a change occurs.
Example
Private Sub SetActivePlottingAlgorithmLinear() TrendPro1.ActivePlottingAlgorithmLinear = True End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal