ActiveMarkerShape property (TrendPro object)

Returns or sets the shape of the point markers for the selected trace. Read/write. Long.
Syntax
TrendPro1
.
ActiveMarkerShape
[ =
value
]
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.
value
- is a Long value that specifies the shape of the point marker. Valid values are:
  • Cross1 = 0
  • Cross2 = 1
  • Circle = 2
  • Square = 3
  • Triangle = 4
  • FilledCircle = 5
  • FilledSquare = 6
  • FilledTriangle = 7
Example
Private Sub SetActiveMarkerShape() TrendPro1.ActiveMarkerShape = 3 End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal