Example: SetStartTimeAndSpan method
Private Sub CommandButton1_Click() Dim DT As Date 'Must set the trend to pause mode. Unable to adjust x-axis time while scrolling Trend1.Scroll = False ' Variable for the XAxis Start Time DT = #10/25/99 10:30:00 AM# ' Set Range to 0 days, 1 hour, 30 minutes, 0 seconds, 0 milliseconds Trend1.XAxis.SetStartTimeAndSpan DT, 0, 0, 1, 30, 0, 0 End Sub
Provide Feedback