RefreshRate property

Returns or sets the rate, in milliseconds, at which the chart data updates. The RefreshRate property applies only when the ChartMode property is set to Automatic. Read/write. Integer.
Syntax
Trend
.
RefreshRate
[
= value
]
where
Trend
- is the name of a Trend object (such as trend1) or an expression that evaluates to a Trend object.
value -
is a parameter of the type Integer that specifies designates the number of milliseconds between data points. Limits are 50 to 2,147,483,647
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal