Example: TimeFormat property
Private Sub GetTimeFormat() If Trend1.TimeFormat = rstTimeFormat12Hour Then MsgBox "The Trend is using 12 hour time format" Else If Trend1.TimeFormat = rstTimeFormat24Hour Then MsgBox "The Trend is using 24 hour time format" Else If Trend1.TimeFormat = rstTimeFormatSystem Then MsgBox "The Trend is using the system time format" End If End Sub
Provide Feedback